Loading

Notes & Terminology

Notes & Terminology hero image
Microsoft Patch Qualifications
  • What's New
  • View Data Tables
  • FAQs
  • Notes & Terminology

Last updated 4/01/2021

Anti-Virus Software (from Detailed Information page) Name and version number of the anti-virus software which was on the machine at the time of the test.
CPR Rockwell software release the Microsoft Patch is installed on.
Date Published The date Rockwell published its recommendation for this MS Patch.
Date Released (from MS Patch Summary and Detailed Information page) This is the date Microsoft released the MS Patch.
Microsoft Priority (Rating) Rating that Microsoft gives each patch, visit Microsoft at https://www.microsoft.com/en-us/msrc/security-update-severity-rating-system to learn more about the rating system.
MS Knowledgebase This is the Microsoft assigned Knowledge Base article ID link to the Microsoft Webpage containing information about this MS Patch.
MS Patch Description This description is produced by Microsoft at the time the MS Patch is released.
MS Security Bulletin (Depricated) This is the Microsoft assigned Security Bulletin article ID number link to the Microsoft Webpage containing information about this Security Bulletin.
Notes Any additional information regarding this MS Patch qualification.
Products A list of Rockwell products tested for this patch qualification.
Qualification ID An internal number used to track all test activities related to this MS Patch qualifications. Any questions regarding this MS Patch qualification should include this number.
  • 联系销售部门
  • 联系客户服务
  • 联系技术支持
  • 电话支持
  • 一般问题
  1. Chevron LeftChevron Left 中国 Chevron RightChevron Right
  2. Chevron LeftChevron Left 支持 Chevron RightChevron Right
  3. Chevron LeftChevron Left 产品支持 Chevron RightChevron Right
  4. Chevron LeftChevron Left Notes & Terminology Chevron RightChevron Right